Tripp Lite

Frequently Asked Questions

Power Problems - Brownouts

Site Map
Model Number Search


Other Resources

Power Protection Glossary
Pre-Sales Inquiries
Technical Support
Product Selectors
UPS Selection Worksheets (PDF)
Where to Buy
Contact Tripp Lite

 
Brownouts
Blackouts | Brownouts | Spikes & Surges | Line Noise
       
  Q:

What is a brownout?

 
  A:

Brownouts are periods of low voltage that can cause lights to dim and overtax equipment. Also known as voltage sags, they are the most common power problem, accounting for up to 87% of all power disturbances.

 
       
  Q:

Where do brownouts come from?

 
  A:

Overburdened utilities sometimes reduce their voltage output to deal with high power demand. Statistics show that the U.S. population tries to pull an average of 5% more power than utility companies can provide.

Damage to electrical lines and other factors can also cause utility brownouts. Locally, equipment that draws massive amounts of power, such as hair dryers, air conditioners, or laser printers, can cause momentary brownouts to occur.

Undervoltages are often followed by overvoltages - "spikes or surges" - that are also damaging to computer components and data.

 
       
  Q:

What do brownouts do?

 
  A:

Voltage variation can be the most damaging power problem to threaten your equipment over time. All electronic devices need to receive a steady voltage (120 VAC in North America and 220/240 volts in many other parts of the world) in order to operate correctly.

Brownouts place undue strain on power supplies and other internal components, forcing them to work harder in order to function. Extended brownouts can destroy electrical components and cause data glitches and hardware failure.

Overvoltages burn out power supplies and other components, and can cause massive damage to your electronic hardware. Extended overvoltages can even cause fires as electronics "fry" in the extra electricity.

 
       
  Q:

How can I protect against brownouts?

 
  A:

Tripp Lite Line Conditioners and Uninterruptable Power Supplies (UPS) are your best defense against both voltage problems.

 
       


Power Protection Solutions for Brownouts


 
Couldn't find the answer to your question here?
Email Tripp Lite Technical Support


© 2009 Tripp Lite. All Rights Reserved.